4/13/2015 1:28 PM | |
Posts: 2 Rating: (0) |
Hi I have configured discrete alarm in TIA portal V13 for s7 1200 plc I have to trigger alarm when my digital inputs turns to 1 and acknowledge when it turns 0. the digital input is given to a add block the output if the add block is MW0. when i turn on the input the alarm shows in hmi and if when i turn off it still displays on the screen i cant acknowledge using the plc tag help me!
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/14/2015 12:24:37 PMNew subject after splitting |
|
4/19/2015 8:29 AM | |
Posts: 5225 Rating: (1185) |
Could this post be of help?... [LINK] |
Follow us on