7/16/2013 7:00 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Agree with you 100%. Cannot imagine life without Teamviewer. I have been able to reduce my travelling by 80% with the use of Teamviewer. My desk these days looks like a mini control room with sometimes upto 3 Teamviewer sessions running on different laptops simultaneously. This way I can assist my team in multiple projects without leaving my office. We have made it as a standard to install Teamviewer on all projects that we commission so that ( as Ayman Elotaifysaid ) we can provide instant support to our customer in case of a problem. Even of the problem cannot be solved using teamviewer, the engineer visiting site can go much better prepared as he can understand the issues before leaving for site. Some great features of Teamviewer that we love are : a) Can quickly see the problem on my Mobile using Teamviewer Mobile, even if I am travelling. b) Can simultaneously Chat with the person at site using built-in chat. c) Can Transfer Important failes and take Backups using built-in File Transfer. d) Can Even Transfer Licenses using the Built-in VPN function Cheers Navnag |
There is no such thing as the last bug in a program |
|
7/16/2013 10:31 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
A lot of portable, free & legal tools, running from a stick: Notepad++ Programmer's Notepad Greenshot PhotoFiltre7 SumatraPDF DatbaseBrowserPortable Cppcheck Portable CCleaner with CCEnhancer VMWare Acronis True Image Hobocopy |
B r g d s , |
|
Follow us on