9/30/2011 2:56 PM | |
Posts: 178 Rating: (5) |
WinCC status and control in the system tray! WinCC has an application which runs in the background that I can see the status of all the servers and clients and their connection status. Would this be possible to embed within a screen on WinCC. The application (Simatic WinCC)can be seen running on the task bar (notification area). Regards, gbs AttachmentMDM_-_WinCC__Configurations_-_WinCC_status_and_control_in_the_system_tray[1].pdf (1036 Downloads) |
Last edited by: gbs at: 10/3/2011 10:37 AMCome on experts, someone must know something... |
|
10/3/2011 11:08 AM | |
Joined: 3/15/2010 Last visit: 4/2/2024 Posts: 137 Rating: (9) |
Please take a look at the screenshot in attachment to see what I mean. |
10/13/2011 12:07 PM | |
Posts: 1530 Rating: (59)
|
Hello gbs, sorry, that I didn't answer to you earlier. |
3/18/2012 7:19 AM | |
Joined: 3/18/2012 Last visit: 12/12/2022 Posts: 1 Rating: (0) |
Dear All, Can i know which is the tag used for this server redudancy status? |
4/16/2012 9:57 AM | |
Posts: 1530 Rating: (59)
|
Hello xelan, maybe this FAQ can help you. Which tags indicate the status of the server. Best regards Bizur |
9/25/2013 11:06 PM | |
Posts: 4 Rating: (0) |
Hello, I am very interested about gbs's question, that is quite old but has still not been answered. Regarding monitoring redundant servers state, there is already a proposed solution, using a PLC: http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=22820491&load=treecontent&lang=en&siteid=csius&aktprim=0&objaction=csview&extranet=standard&viewreg=WW However I would like to check the possibility of not using a PLC to check these states. And this "Computer List" that WinCC shows on system tray seems to be the solution. If the station can show the states for both redundant servers, there has to be a way to do this check through WinCC. Does anyone know how this application checks those states? Thanks, Ricardo Gondo |
Follow us on