4/30/2016 2:06 AM | |
Posts: 111 Rating: (1) |
I have different machines in the plant and I am displaying the Text message on the big TV when any machine goes on fault. I am using a text field and displaying a text when there is a fault by using fault bits from the machines. I am using TP2200 HMI for this and displaying HMI on big TV and it's working great through runtime. I am having a problem when 2 machines goes down at the same time then I am getting a fault of machine that goes down first. What can I do to display all the faults at the same time because I am putting text over each other and when the machine goes on fault that text appears flashing but if another goes down so I want to display that text as well like one fault flash and then other fault flash and if there is 3rd fault then it should be appear as well. I am trying to summarize that I want to display fault message one after another continuously flashing until machine gets fixed.
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 5/2/2016 9:53:13 AMNew subject after splitting Last edited by: The Helping Hand at: 5/2/2016 9:54:40 AMRenamed the thread title |
|
5/2/2016 6:44 PM | |
Posts: 111 Rating: (1) |
You mean manage the switching of faults with PLC? Because this is what I am looking for to manage the switching between faults. |
5/2/2016 7:23 PM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:10:48 AM~(‾▿‾)~ |
|
5/5/2016 7:46 PM | |
Posts: 111 Rating: (1) |
Any suggestions? |