8/31/2020 3:27 PM | |
Posts: 3 Rating: (0) |
Anyone can help? |
8/31/2020 4:52 PM | |
Joined: 9/27/2006 Last visit: 5/8/2024 Posts: 12257 Rating: (2666) |
Hello nayeem; The screenshot below shows the difference between expansion modules (with IM 360/361 pairs) and distributed I/O stations, using the integrated Profibus-DP port on the 2 CPUs you mention. You can look at chapter 8 "Interface Modules" in the S7-300 Module Data manual to get the specifications for an IM 360/361 used to create expansion racks for an S7-300 CPU. The special cable 368 for IM 360/361 is limited to 10 m max, and the IM 360/361 are used mostly to connect additional S7-300 modules is separate but close-by cabinets. https://support.industry.siemens.com/cs/ww/en/view/8859629 Profibus-DP (or Profinet) networks use the integrated Profibus (or Profinet) ports of the CPU, or specialized CPs, such as CP 342-5 for Profibus and CP 343-1 for Profinet, to connect to distirbuted I/O stations that can extend much further than expansion rack scenarios, and use different types of I/O families depending on the local requirements. You can have an idea of available types of ET 200 (distributed I/O) stations in this document; https://www.elfadistrelec.no/Web/Downloads/_b/ro/siemens_simatic-et200_eng_bro.pdf So, after this introduction, to your specific questions: -1. You can communicate as you describe with distributed I/O stations through Profibus (or Profinet), as discussed before. You can even connect 2 Profibus masters on Profibus with a DP/DP coupler, or on Profinet with a PN/PN coupler. Note that there are limitations on what the second CPU can do with the I/O, we can discuss this later, when you are more familiar with Profibus-DP and Profinet.. These documents will show you the range of Profibus and Profinet hardware available for connections on the plant floor (we can help you select the materials when you have advanced further in your project deployment): SIMATIC NET PROFIBUS Network Manual System Manual https://support.industry.siemens.com/cs/ww/en/view/35222591 SIMATIC NET: Industrial Ethernet/PROFINET Industrial Ethernet https://support.industry.siemens.com/cs/ww/en/view/27069465 -2. The I/O addressing for Profibus-DP or Profinet modules is the same as if the I/O were in the same rack as the CPU. The I/O is seen as part of the process image or the peripheral modules of the CPU.(see answer to point 4) -3. This training manual will show you step-by-step example of setting up a Profibus-DP connection between a S7-315-2DP with a ET 200M station (ET 200M: IM 153-2 with S7-300 I/O modules): -4.The document cited above, on page 15, for example, shows how the remote station DI and DO modules (on the ET 200M) are attributed "normal" addresses inside the process image tables of the CPU. You will find more detailed information in the following manual: SIMATIC Configuring Hardware and Communication Connections STEP 7 https://support.industry.siemens.com/cs/ww/en/view/109751824 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 08/31/2020 21:30:10Last edited by: dchartier at: 09/01/2020 15:07:27 |
|
Follow us on