10/3/2019 4:58 AM | |
Posts: 35 Rating: (3) |
Ok will try that tomorrow. Thx!! |
10/10/2019 3:21 AM | |
Posts: 35 Rating: (3) |
I was able to reset the NCK and that stopped the 65536006 MDA buffer error. Now I can write into the MDA window and issue commands. Still get the mbdde.ini error at start and when i try to view alarms, I get the MBDDE.EXE cant start error. UPDATE. Fixed all the errors by expanding the ARJ archive on a mac OSX machine. Took system drive and connected to Mac via USB to IDE adapter. Copied the expanded mdbbe.ini file from the mac to drive and overwrote the original. Now all errors are gone and the error log works again! {snip} ---------------------------------------------------------------------- Additional question posted twice - please use: Cant load PLC archive in 840D MMC103
|
Last edited by: The Helping Hand at: 10/11/2019 16:13:57removed question which was posted twice. Last edited by: SurvivalResearch at: 10/16/2019 01:41:46Last edited by: SurvivalResearch at: 10/16/2019 01:42:30Last edited by: SurvivalResearch at: 10/16/2019 01:42:58Last edited by: SurvivalResearch at: 10/16/2019 01:43:26 |
|
Follow us on