Industry Online Support
Technical Forum
9/16/2016 7:08 PM | |
Posts: 20 Rating: (0) |
I'm using a Do-More and a Leuze laser distance sensor to monitor a large hydraulic cylinder. I have to calculate and log the velocity. I have tried to capture a reading based on a 50ms or 100 ms clock the move that to a R location then capture a second and move to another R location then do the math between the two and do the calculation... I cant get it to work. Does anyone have a suggestion on how to get there>> the fastest the cylinder could be moving is 17'/sec. the stroke is 5' |
9/16/2016 8:38 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22250 Rating: (2984)
|
sorry but I think you are in the wrong conference and in the wrong forum Do-More PLC and Leuze are no products from SIEMENS so I think is hard to get any help here in the SIEMENS Forum! |
Follow us on