9/7/2017 8:38 AM | |
Posts: 26 Rating: (0) |
Hello Will this work with S7300 PLC? Does it support comms as PG/OP or it uses only TCP/IP ? I ask because in addition to S7300 I also have VIPA plc that have only PG/OP comms enabled. Will it work? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/7/2017 12:26:03 PMNew subject after splitting |
|
9/7/2017 4:00 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi, yes the S7 node works with a S7-300 PLC as well. To be honest I do not know what PG/OP exactly is. But as mentioned on the github page of the s7 node the nodes are working via ISO-on-TCP. Maybe you can find some additional information on this page. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on