11/29/2016 12:03 AM | |
Posts: 33 Rating: (2) |
Does PCS 7 Advanced Engineering v8.0 works with PCS 7 v8.2? How can I get Logic Matrix addon? It is not available on PCS7 v8.2 DVDs. |
11/29/2016 7:23 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Dawg1, Yes, it does work, however there is a footnote: - Advanced Engineering System v8.0 SP1 works with PCS7 v8.2 - Advanced Engineering System v8.0 SP2 works with PCS7 v8.2, but you will need CFC Upd2 installed I stop using Advanced ES because Siemens is working on a new concept called: PCS7 Automation Base. Link to manual: PCS7 Automation Base. The manual exists, but the software is not released (I don't know when). It will use the Control Module Types concept. Since v8.1, Advanced ES is not supplied anymore with the DVD. The Logic Matrix should be enclosed with the software media package. At least I have it in my version: 6ES7658-4XX28-0YT8. It is the EU version.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on