6/18/2017 12:57 AM | |
Posts: 1 Rating: (0) |
So I´ve recently been getting the backups of every Siemens HMI we have at our plant, however most of the panels have their own MMC attached to them (which as far as I know has some récipe data, the pdz file and...?), so my question is: If I get a backup from WinCC (backtransfer) and/or with Prosave, does that backup include the contents of the MMC? If the HMI were to fail, when changing the HMI, I would need to move the MMC to the new panel? or in case of MMC/HMI failure, I could just put a new MMC, start the restore and all the contents would be there? If these backups dont include the MMC, how do I get a backup of the MMC?, just plug it into a PG and copy/paste its contents? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/20/2017 6:07:20 PMNew subject after splitting |
|
6/22/2017 2:24 PM | |
Posts: 648 Rating: (95) |
Hey Edgmarb, these FAQs could be helpful for you:
With best regards rh1990 |
Follow us on