7/22/2017 11:55 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi again Well, the creep flow means the flow in states: End, Off and Pause.. It's the flow which is measured, but unintentially. You can turn this off when setting Featurebit 13 from 1 to 0. If the FeatureBit is 1, creep flow is always detected in the dosing quantity. If the FeatureBit is 0, the creep flow is only detected when CR_AH_Lim is reached. But as for all analog blocks, you can turn this completely off when setting CR_AH_En to 0. The creep flow does not have any effect in affecting the dosing quantity. |
If I could help you, you can use the RATE button. Thank you. |
|
12/16/2022 7:57 AM | |
Joined: 11/16/2019 Last visit: 12/20/2022 Posts: 1 Rating: (0) |
Hey, since it has been more than 5 years since your last answer, did you solve this issue? Thanks |
Follow us on