12/3/2019 4:05 PM | |
Joined: 11/10/2010 Last visit: 8/29/2024 Posts: 170 Rating: (9) |
Hello Heisenberg2, there's any issur to do the oppsite and downgrade the firlmware of an AS in case i will buy a new AS and the PCS7 version of the system is 8.1 and can't be updated in this tiime ,so may be i can buy a new AS and downgrade the firmware for use with PCS7 8.1 !? thank you ------------------------------------------------------------------------------------------ |
Last edited by: Ahmed.tn at: 12/03/2019 16:06:29Last edited by: Jen_Moderator at: 12/04/2019 10:18:48New subject after splitting |
|
12/18/2019 4:58 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Autogen, not sure which cpu are you referring to, but below link is for CPU410-5H You may also search the firmware using the below links Attached with a picture on the method of searching in siemens platform |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
12/18/2019 7:47 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello AutoGen_8765335, as addition to the post of JazTai
you can find an overview with firmware for the CPUs 41x at follow link: With regards |
Follow us on