8/26/2020 8:19 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, It sounds like a strange problem.. it helps if you have some print screens from the FB (in online view) and from the WinCC download error. In general I doubt a FB can mess up the OS project. Could be a problem in the project (corrupted somehow). What I suggest is that you take the APL Example project which you can open from Simatic Manager when opening multiprojects, select the "Example" tab. Try to see if you can download the project to AS and OS. There are a lot of steps you must take to accomplish communication between AS-OS - Create PC and PLC stations in hardware and download PLC station - Configure NetPro , merge IE network and download - Configure PC station for use with named connections through Station Configurator (Configure+Download) - Enter the correct PC station settings like OS name, path to OS project. - Configure the OS project (redundancy settings, timesync, user administration, run OS project editor - Configure Simatic Shell on each system - AS compile + download, then OS compile + download. Probably forgetting some steps, but it requires some effort. Easiest thing is to take the example project and start from there |
If I could help you, you can use the RATE button. Thank you. |
|
8/26/2020 9:54 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Sounds like a problem with the installation. Can you share the installed software and possibly answer the questions which are posted in the following topic: The steps to get the installed software are described in the topic. |
If I could help you, you can use the RATE button. Thank you. |
|
8/26/2020 10:06 AM | |
Posts: 39 Rating: (0) |
Installed software on ES Windows : Windows 10 Enterprise 2015 LTSB Version 10.0 (Build 10240) |
Last edited by: morylATCS at: 08/26/2020 10:08:34 |
|
8/26/2020 10:19 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
No, it means the configured OS name is different from the one you are working on. is not the cause. |
If I could help you, you can use the RATE button. Thank you. |
|
8/26/2020 10:21 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Can you upload all txt files in a zip file from the following directory on the ES and OS PC: C:\Program Files (x86)\Siemens\WINCC\diagnose. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on