Industry Online Support
Technical Forum
2/26/2009 11:42 AM | |||||
Posts: 124 Rating: (17) |
Hello Ralphtang Here are two FAQs about this thema (one CPU is Master and the other is Slave). It can be used with two CPU 315-2 DP but the DP Port cannot be Master and Slave ate the same time. So if you have slaves in the port you need another Profibus interface (CP).
Remember that you could use also a DP/DP Coupler or Global Data Communication through MPI or even Ethernet Send Receive. Regards Mario Braganca |
||||