6/15/2012 10:07 AM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Dear mexflexx, Drive ES PCS7 Libraries don't provide the routing functionality. For routing, Drive ES Basic is necessary. Ifthe latestSINAMICS drives are used with the old PCS7 versionplease consider, that perhaps a update to the DES PCS7 6.0 SP2 is needed http://support.automation.siemens.com/WW/view/en/18495518and the "HF1 for Drive ES PCS7 V6.0 SP2 for the extension of the product portfolio of the SINAMICS drives supported" http://support.automation.siemens.com/WW/view/en/52536369 Please refer to the Drive ES PCS7 compatility chart http://support.automation.siemens.com/WW/view/en/18495518anyhow. Best Regards |
With best regards, |
|
6/15/2012 10:15 AM | |
Posts: 14 Rating: (0) |
actually im using mm440, G130/150 |
Follow us on