12/6/2019 4:25 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Which is PLC CPU or control? Please refer this link wherein you will find application examples. HTH |
12/6/2019 2:57 PM | |
Joined: 9/17/2015 Last visit: 8/12/2024 Posts: 137 Rating: (4) |
I am using a NC unit with PLC 317F-3 PN and I am updating a old project with addition parts I am attaching my hardware configuration. When I add a drive (GSD file) in HWConfig, I do not get an option to commission this drive in starter V4.4 AttachmentStation View.zip (90 Downloads) |
Last edited by: Divej93 at: 12/06/2019 22:09:38 |
|
12/9/2019 2:53 PM | |
Joined: 9/17/2015 Last visit: 8/12/2024 Posts: 137 Rating: (4) |
Hi, The NCU MLFG No. is 6SL3040-1MA01-0AA0 FW V5.2. Software Installed is Simatic manager V5.5 SP3 HF11. The version is not available in hardware catalog for Starter and simatic Manager, So I installed the GSD. please see the attached images. when I try to add a Profinet device in Simatic Manager, I cannot see the version even after installing the GSd files AttachmentStarter Version file.zip (86 Downloads) |
Follow us on