1/20/2010 3:34 PM | |
Posts: 739 Rating: (55)
|
Hello, As first you have to know which drive do you want to use. MICRO-/MIDIMASTER = 6se32…….. are not longer available. MICROMASTER 6se64…… still available, to control it you must have a PROFIBUS module 6SE6400-1PB00-0AA0 SINAMICS G120 6SL32 ……. Newest product with CU240S DP the connection to PROFIBUS is possible. To change DC-drive into AC-drive you need to know, the input (supply) voltage, and the needed load (kW); on AC-dive you can’t control DC-motors, you have to change also the motors from DC to AC. And here are some links: Catalogs: https://www.automation.siemens.com/sd/portal/html_76/support_kataloge.htm?HTTPS=REDIR Handbooks MICROMASTER: http://support.automation.siemens.com/WW/view/en/10804923/133300 FAQ MICROMASTER: http://support.automation.siemens.com/WW/view/en/26424185 Handbooks SINAMICS: http://support.automation.siemens.com/WW/view/en/22339653/133300 FAQ SINAMICS: http://support.automation.siemens.com/WW/view/en/26436769 |
This contribution was helpful to1 thankful Users |
1/21/2010 9:25 AM | |
Posts: 20 Rating: (0) |
the current installed drives are non siemens UNI DRIVE |
1/21/2010 10:31 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Dear zolti103, I think the following FAQs will help you: Where can I find up to date GSD files for using PROFIBUS with MICROMASTER 4? |
Ayman Elotaify |
|
Follow us on