7/16/2010 9:31 AM | |
Posts: 4 Rating: (0) |
Sorry, you can find attached the missing datasheet. The application is for a drum forming unit. These motors are for the refiner and the mill infeed. This is a new unit. I am still in the design phase and I want to select the appropriate drive.
AttachmentBinder1.pdf (825 Downloads) |
7/16/2010 11:45 AM | |
Posts: 4 Rating: (0) |
Can we drive them with SINAMICS? It is mentioned that with the motor there a Hall Effect type encoder. How can this encoder be connected to the drive? |
7/16/2010 12:05 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hi A.H., With Sinamics I don't think it is possible, as Sinamics is specialy meant & designed to work with Siemens motor with special connectors. With Siemens 611U drive it may be possible. Do you have Hall effect encoder interfacing details?, which shall help to check the interfacing possibility. However pls check this link. This may help you. http://www.automation.siemens.com/doconweb/content.asp?item=&cd=SINAMICS_1109_E&scope=all DEEP. |
Last edited by: DEEPSTR2010 at: 7/16/2010 12:12 PM |
|