9/2/2019 2:08 PM | |
Joined: 10/20/2011 Last visit: 4/24/2024 Posts: 1 Rating: (0) |
Hallo during the installation of the update 3 for V15.1 I had few problem, then I uninstall V15.1 and when I installa I had this error : 11:48:25 |ERROR AdsWorkerForeignExe::GetInstallResult(): - 120: assuming unknown error, because return value <> 0 and either OK- nor ERROR-values are defined. Please check the corresponding log file for more detailed information 11:48:25 | FAIL! StartApplAfter (TIAP15_1::[INSTALLDIR]BIN\SIEMENS.AUTOMATION.GENERATOR.FRAMEWORK.EXE)Failed someone can help me? thanks ------------------------------------------------------------------------------------------ AttachmentSIA_STEP_7_PRO_WINCC_PRO_V15.1@19-09-02_11-36-10_summary.txt (346 Downloads) |
Last edited by: Jen_Moderator at: 09/03/2019 09:51:59New subject after splitting |
|
This contribution was helpful to1 thankful Users |
3/3/2021 5:45 PM | |
Posts: 1 Rating: (0) |
I have the same problem...If you find something pls tell me Thank you... |
3/8/2021 4:39 PM | |
Joined: 3/2/2016 Last visit: 4/2/2024 Posts: 72 Rating: (14) |
Hello, Please try to download and install the KB3033929 from Microsoft at following URL: https://docs.microsoft.com/en-us/security-updates/SecurityAdvisories/2015/3033929 Install KB3033929, reboot your Windows and start a repair installation of STEP7 V15. Hope it helps!
|
7/22/2021 7:01 AM | |
Joined: 2/22/2017 Last visit: 9/4/2023 Posts: 1 Rating: (0) |
Did it work ? |
8/18/2022 1:01 AM | |
Joined: 9/10/2015 Last visit: 4/20/2024 Posts: 5 Rating: (0) |
It is didn't work =( |
Follow us on