5/5/2022 1:15 AM | |
Joined: 5/5/2022 Last visit: 5/8/2022 Posts: 1 Rating: (0) |
It doesn't seem to fit. DXR2 controllers are used to automate small systems such as fan coil and radiator. Peripheral devices are directly connected to the input and output terminals of the controllers. The model range contains controllers with communication via BACnet\IP and BACnet\MSTP. Both AC 24 V and AC 230 V power options are available.A full description of the inputs and outputs of the controllers is available in the technical documentation. You can also get a waterproofing work with the help of special services that provide similar services. |
Last edited by: timotygreg at: 05/08/2022 16:35:06 |
|