Industry Online Support
Technical Forum
6/24/2009 4:00 PM | |
Posts: 45 Rating: (8) |
Hi, Try to use ANY parameter type instead of POINTER. You can change ANY pointers dynamically and settle them on address and length you need Best regards |
6/24/2009 4:46 PM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello, when you use theinput parameter of the type POINTERfor both arrays then you get exact pointer to the start address of each array. If you need also the length (suppose yes) then use the ANY pointer as SSE suggested and by parsing of it you could get the length. For detailed information about these data types look at the Step7 online help. Also some discussion about the pointers is for example here, if you search the forum you get also another threads. Regards Sydney |
Last edited by: Sydney at: 6/24/2009 4:48 PM |
|