Industry Online Support
Technical Forum
4/30/2011 3:02 PM | |
Joined: 8/25/2006 Last visit: 4/24/2024 Posts: 2203 Rating: (277)
|
Hello. To avoid this error note that total load of all 5 cyclic tasks should be less then 100%. So you need to reduce the load of some cyclic task so that the total load will be lower then 100%. In your case especially look at load of T3. And remember that load of T1 affects on load of all other T2-T5, load of T2 affects on load of T3-T5, and so on. Also look at this thread where the same problem was described. |
Follow us on