12/2/2019 11:16 AM | |
Joined: 9/9/2014 Last visit: 3/26/2024 Posts: 242 Rating: (40) |
I already answered your question in the controller section - 300 series And as I said - there is no difference which software you use - it all depends on the modules. More advanced fault analysis options are available for the 1500 Series (more advanced diagnostics) for example - See the manual below: SIMATIC S7-1500/ET 200MP Digital Output Module DQ 16x24VDC/0.5A ST Manual clipping: ************ 5.2 Interrupts Diagnostic interrupt The module generates a diagnostic interrupt at the following events: For more information on the error event, refer to the error OB with the "RALRM" instruction ************ This only confirms my words, voiced in the same past topic. If my answers helped you, close the topics, put a rating. Thanks in advance! |
Last edited by: Unreality at: 12/02/2019 11:16:51Last edited by: Jen_Moderator at: 12/02/2019 11:32:42Optimized link. Best Regards |
|
This contribution was helpful to1 thankful Users |
Follow us on