Industry Online Support
Technical Forum
6/11/2013 2:05 PM | |
Posts: 391 Rating: (50)
|
Hello, in the attachment there are a couple of examples tested on Sinumerik Operate 4.5 SP2: param_grid uses a GRID to display BYTES and BOOLS Please note that the manual states that the values in the table should be of the same type, so this example is out of standard.... but it seems to work param_index is an alternative to the GRID: you define an additionalvariable and use it as an index to scroll through the values. You can add more input fields to the page to have more variables and minimize the need for scrolling. DB100 was declared asan array of 100 INT (i.e. 200 bytes), but the example works also with structures becauseyou always have to use the absolute address of the variable anyway. AttachmentF:\forum\GRID_EASYSCREEN.zip (150 Downloads) |
Follow us on