1/23/2017 6:24 AM | |
Posts: 3 Rating: (0) |
I am using Simatic Manager Vs5.5 and also disable the Antivirus. I ping all devices and all are ok. But still whenever I browse devices in Edit Ethernet Node. Its not showing anything. So please help to solve out this. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/23/2017 12:00:29 PMNew subject after splitting |
|
3/6/2017 9:34 AM | |
Posts: 3 Rating: (0) |
I was trying to connect it through Switch. But i also tryed to connect directly to PLC. but still i faced the same problem. |
3/25/2017 8:18 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Edit Ethernet Node should be a simple function to detect available node connected to your station. Is there a bug? Or is it because of the PG/PC interface was not set properly yet? For the first time to detect the PLC, we suppose to set the PG/PC interface directly to the network adapter of the local station and not PC internal local. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on