12/5/2010 3:55 PM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (353) |
Hi, If you are "looking to add a small addition to the PLC on one of our CNC Machines with an 840D control.and looking to use afew inputs &outputs, atimer and alarms take it easey, try this 1st: add FC200 (ANY NUMBER is free you can use) FC200 A Ixx.0 =Qyy.1 BE then add in OB1 call FC200 (or you can: UC FC200if FC200 no parameter) SAVE and download to PLC test if the function works when it is OK, then you can do more you want that should be OK. if you meet any alarms or messages.post them then there will be someone can help you good luck! [schnippschnapp] new question is splitted to I''m looking to add a small addition to the PLC on one of our CNC Machines with an 840D control. |
Last edited by: O_Moderator at: 12/8/2010 9:21 AMLast edited by: nulizhang at: 12/5/2010 3:56 PMIf you like my comments please |
|
Follow us on