12/22/2011 3:56 PM | |
Posts: 4 Rating: (0) |
Iwant to find out how i can run a motor to 60 hz ? what effects will be there if one runs a 50hz rated 400KW motor upto 60Hz? |
12/22/2011 4:47 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Hello, I think it's all explained here : http://www.eng-tips.com/faqs.cfm?fid=1224 Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
5/15/2012 10:18 PM | |
Joined: 6/4/2008 Last visit: 9/15/2024 Posts: 1497 Rating: (324)
|
Hi, the attached describes the effects for G120 and MM4 drives, but to be fair, this is applicable to any drive/motor combination. Hope this answers some more questions. Regards, Graeme
AttachmentPDF_Operating_motors_at_higher_frequencies_V2_en.pdf (1760 Downloads) |
This contribution was helpful to2 thankful Users |
11/7/2017 3:04 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Jengeese is split to a separate thread with the subject Motor with a plate "30 kW 400 Volts 50 Hz 1475 rpm" - Is it possible to run it with same motor drive but in 2248 rpm?. Best regards |
Follow us on