Industry Online Support
Technical Forum
8/1/2013 6:30 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hi ashishm Unfortunately S7-200 can only be a Profibus Slave using EM277. You would need it to be a Profibus Master if you want to control AB Drives on Profibus. Unfortunately there is no way of doing this in S7-200. These has been discussed in several previous posts. You can check out : /tf/WW/en/Posts/42743 /tf/WW/en/Posts/31226 You can consider using S7-1200 which can be a Profibus Master or Slave. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on