5/31/2014 11:15 AM | |
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
hey ucon89, did you read Tips and tricks for printing trends and reports in WinCC? Also try checking WinCC logfiles in "C:\Program Files\Siemens\WinCC\diagnose\" for more possible details. |
B r g d s , |
|
5/31/2014 11:20 AM | |
Posts: 691 Rating: (37) |
Dear ucon89 Have you created proper Report Format in the Report Layout. Use proper control Tool in the Report Designer and then assign the print Jobs |
5/31/2014 9:32 PM |
|
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
Hey Kiran Dabhi, is it possible that your Caps Lock-button is stuck? You know that writing all capitals in a forum is considered as shouting? Just for your information anyway, thanks for the reply. |
B r g d s , |
|
6/1/2014 7:43 AM | |
Posts: 67 Rating: (1) |
Yes, I had read it. But still not help.
What do you mean? Can you explain bit more? I use standard print. When I click on RunTime, the data of print is come. But, when I set hourly in report designer, the data is not there, only the layout had printing. |
6/1/2014 7:54 AM | |
Posts: 691 Rating: (37) |
Dear ucon89 Please rectify me , if I am not wrong. You have created a report page with some values in it. You have assigned that report layout with a print job. That print job is set hourly to print. By doing all these, you are able to print from the Runtime Window, but you are not able get the values in hour basis. Please upload the snapshot of thr runtime reports and the print format. |
6/1/2014 8:14 AM | |
Joined: 6/8/2013 Last visit: 7/18/2024 Posts: 158 Rating: (9) |
It is possible through script |
6/1/2014 12:21 PM | |
Posts: 67 Rating: (1) |
Bold. yes correct. When I print (click button) on Runtime the print is normal and data show. But when I set to hourly, the print is normal too but the data is not show. I do not understand what you mean of the snapshot, because the difference only runtime has data, hourly report has not data. |
Follow us on