4/11/2017 3:39 PM | |
Joined: 8/7/2014 Last visit: 6/10/2024 Posts: 13 Rating: (0) |
Hi, I am also using similar configuration with TIA V13 with S110 and S7 1214C, it worked in starter but when i am connecting via TIA with Technology objects it showing Encoder error while commissioning is there any limitation for 1214C, Can somebody share sample program with technology object with 1214C., Thanks in Advance, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/12/2017 2:12:06 PMNew subject after splitting |
|
4/12/2017 2:14 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
The second thread with the subject not able to use Technology ojects in S7 1214C with TIA 13 V SP1 is located within the conference STEP 7 (TIA Portal). Best regards |
Follow us on