Industry Online Support
Technical Forum
9/10/2010 1:11 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
what denzilg_sa said is absolutely right about single encoder for two drives
Now regarding your another Qn, yes you can use drive without Encoder too. You can use SLVC (P100=3 incase of VC drives) or V/F control (P100=1 for VC) Control mode should be selected depending up on application. I already mentioned which parameter you should change...
For this, check some basics like Isolation of Encoder cables from Power cables and Etc... Also Refer this... Trouble shooting in Vector Control Mode Best Regards, Devesh Vithani |
Last edited by: Vithani at: 9/10/2010 1:15 AMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on