Industry Online Support
Technical Forum
6/27/2008 11:25 AM | |
Posts: 2348 Rating: (264) |
Could you post your test code here ? |
6/27/2008 3:21 PM | |
Posts: 2348 Rating: (264) |
Function is really called? Can you see this CALL on monitoring block? Redownload it to PLC from library |
This contribution was helpful to1 thankful Users |
6/27/2008 5:24 PM | |
Posts: 2348 Rating: (264) |
I'm sure it could^) Please note 1MBismaximumfilesizeyoucanuploadhere. |
7/1/2008 9:23 AM | |
Posts: 7 Rating: (0) |
This is the testversion that I used. FC41: In network 3 are the Find, EQ_string and NE_string that gave problems. M20.1 and M20.2 are the bits that I could set and reset without being overwritten. I also tried using just 1 network with the EQ_string function so that it won't be influenced, but still not the result that I wanted. Attachmenttest.zip (267 Downloads) |
7/1/2008 8:13 PM | |
Posts: 121 Rating: (16) |
If a called block is green it only indicates that the RLO? is true. This makes the block turn green when monitoring. Try youre self //Green SET SAVE //Grey CLR SAVE |
Follow us on