9/9/2014 3:47 PM | |||||||||||||||
Joined: 9/27/2006 Last visit: 5/13/2024 Posts: 12257 Rating: (2668) |
Hello Ignacio; If you need to document the type of memoryre quired by your different CPUs, use the search box at the right of this page, with the part number of the CPU as a searh term. You will find the CPU part number on the front of the CPU, for example. Once you have reached the Product Support page for your CPU, open the Technical Data tab, and look for the "Backup" section. Here are the contents of that section for 2 different models of CPU 315 so you can see the differences, one from the end of the 1990s, the other more recent:
This model requires a support battery, look at this FAQ for more details: What are the order numbers of the back-up batteries for the various CPUs?
You do not need a support battery for this CPU, but you must have an MMC of adequate size. Hope this helps, Daniel Chartier |
||||||||||||||
Last edited by: dchartier at: 9/10/2014 1:36 AM |
|||||||||||||||
9/9/2014 4:01 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Ignacio, and for IM151-8 PN/DP e.g. 6ES7 151-8BA00-0BA0 no need battery Manual wrote: Backuphis is a ET200sBackup present Yes ; Ensured by SIMATIC Micro Memory Card (maintenance-free) |
Last edited by: Ste39 at: 9/9/2014 4:10 PMLast edited by: Ste39 at: 9/9/2014 4:01 PM |
|
9/9/2014 4:08 PM | |
Posts: 7 Rating: (0) |
This forum is simply wonderful! Thanks for your help! |
This contribution was helpful to4 thankful Users |
2/5/2018 11:35 AM | |
Joined: 6/19/2017 Last visit: 5/14/2024 Posts: 8039 Rating: (164) |
New question published by Sylko is split to a separate thread with the subject PLC does not keep the parameters entered after 24 hours maximum. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on