9/4/2009 3:02 PM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi Cosh , Error 443 means you didn't configure "F_TYPE" parameter in IEPH CFC block. I seen you configred blocks like v4.2: that blocks version are coming from Batch Flexible (PCS7 v4 & PCS7 v5). If you are using new IEPH CFC blocks, jst need configure parameter F_TYPE in the block. If you migrated Batch Flexible database in new SIMATIC Batch version keeping old AF_x CFC blocks in PLC programs, no changes can be done but only delete change AF_x bloks with new IEPH function. Hope can help Regards |
9/4/2009 4:48 PM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hello Cosh , you right. no possible to find F_TYPE parameter when you use SFC Type function. so...i think problem should be the original SFC Type version, but only if you got SFC fromolder PCS7 version (because SFC interface -FB300, @SFC_RTS- changed). doesn't matter if you developed SFC Type on different station if same PCS7 version used.
I think SFC has been developed with different PCS7 version Hope can help Regards |
Follow us on