12/12/2008 11:02 AM | |
Joined: 9/16/2008 Last visit: 8/29/2024 Posts: 56 Rating: (0) |
Hi, I've a PLC Backup for that Simatic Mangaer V5.4 + SP4, Win CC v 6.2, Win CC Flexible, Simotion and CFC V6.1 is required. I've installed everything. I've also installed the Additional Softwares from Win CC for Excel Comunication. However There is an Error stating "WinCC (Component Object Manager) " in the Software Package Missing window. Can any one give me any solution. What need to be installed? Hardware compilation cant be possible because of this error. Here I've attached the print scrren of the above error. AttachmentS7 Error.zip (194 Downloads) |
12/12/2008 12:00 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Component Object Manager - This allows the insertion of the WinCC objects into Simatic Manager. Are you sure that you have installed copletely packet of WinCC ( with marked all component )? See here Wie kann ein vorhandenes WinCC Projekt in ein STEP 7 Projekt integriert werden? You can add this options by clicking add/remove components for WinCC. regards |
12/13/2008 5:54 AM | |
Joined: 9/16/2008 Last visit: 8/29/2024 Posts: 56 Rating: (0) |
Hi Umencho, Thank you for your suggestion. |
Follow us on