Industry Online Support
Technical Forum
5/8/2009 12:38 PM | |
Posts: 15 Rating: (0) |
Dear all, I was having WinCC flexible 2008 installed in my PC and then I tried to install WinCC V6.2. Before that I tried to install MS SQL server 2005 but it shows error during installation that other same program is running at the same instance. I, then, uninstalled SQL and all components and removed it from registry. It continued showing error. And finally I uninstalled WinCC flexible 2008 as well. I read FAQ and deleted "WINCCFLEXEXPRESS" folder. But still the problem remains same, I am not able to install SQL server 2005 and the log file is as attached. Could anybody guide me that how to resolve this problem?? Regards. AttachmentSQLSetup0003_THINKCENTRE6_Support.zip (81 Downloads) |
5/8/2009 2:01 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello, here a FAQ .... http://support.automation.siemens.com/WW/view/en/30576253 regards manfred |