2/27/2008 7:20 PM | |
Posts: 15 Rating: (0) |
Hi everybody. I have a problem will using User Archive in WinCC V6.2. I have a fresh copy of Wincc V6.2 installed in my pc. All other projects except the project in which i have selected "User Archive" Option in Computer option in Wincc explorer works fine. I created a new project with only one graphic page and no user archives in it as shown in PIC:-01 and PIC:-02. Please refer to the attachment. This project can be put to runtime and can be stop if i have not select "User Archive" Option. Once i select the this option as shown in PIC:-03 and try to put it in runtime, the project hangs up with an error message as shown in PIC:-04. Then i have to make it off by "Task Manager". If now i try to open the same project error report as shown in PIC:-05 appears. And i m not able toopen the project again. Can anybody help me. Thanks in advance. Patel Divyang. AttachmentWinCc Archive Problem.pdf (59 Downloads) |
Follow us on