Industry Online Support
Technical Forum
12/17/2008 2:35 PM | |
Posts: 325 Rating: (13) |
Hi, I have bit of problem when I put the attached VB script in WinCC. Basically this script records the average of tags in an hour & stores in a data file. The message I get during syntax check is " expected end of statement". Need some help!!!! Regards Nil AttachmentMacro1.pdf (72 Downloads) |
12/17/2008 4:42 PM | |
Posts: 68 Rating: (0) |
Sorry, But this is not VB Script code. It's Visual Basic code. That's the reason for thesyntax error. |
Follow us on