6/28/2010 10:39 AM | |
Posts: 4 Rating: (0) |
hi. I can´t load microwin v4.0 .....v4.7 on xp sp3 because stop the load at 90% .....ERROR CAN¨T LOAD DEVICE DRIVERS. Please i need yours help, thank you |
6/28/2010 11:02 AM | |
Posts: 4 Rating: (0) |
thanks... i have on my pc step7,protool,starter,simo drivers.....without problems..... i think so is problem the xp |
6/28/2010 11:45 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Dear arw, Please have a look at this link: Which version of Step 7 Micro/Win or S7-200 PC Access is compatible with which version of MS Windows? So Windows XP + sp3 is released for version V4.0 + sp7. Best regards, Wizard |
6/28/2010 11:51 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, If you mean STEP 7-Micro/WIN V4.0 Service Pack (SP7) -
So, try How to uninstall STEP 7-Micro/WIN V4.0 after aborted installation? and then start again installation. If you are sure (you did it before) in "healthy" of installation files then should be OK. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
6/28/2010 12:22 PM | |
Posts: 4 Rating: (0) |
THANKS..... BUT NO WORKING.......V4.0 + SP7 ALL IS EVIL!!!!! always same error at 90% device drivers error THANK YOU VERY MUCH |
6/28/2010 12:26 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Dear arw, Have you tried to uninstall Step 7 Micro/Win, like UMENCHO said? Best regards, Wizard |