11/15/2019 7:57 AM | |
Joined: 7/22/2014 Last visit: 3/24/2024 Posts: 66 Rating: (2) |
I also have the same error message when I re-compile a project with Scout V5.2 |
11/16/2019 7:44 PM | |
Joined: 6/4/2008 Last visit: 5/1/2024 Posts: 1484 Rating: (322) |
Thanks Christoph, that worked a treat, as ever, You are a Legend! Regards, Graeme |
11/18/2019 1:19 PM | |
Joined: 11/21/2017 Last visit: 4/11/2024 Posts: 1 Rating: (0) |
Thank you!
|
11/21/2019 10:50 AM | |
Joined: 4/24/2019 Last visit: 4/30/2024 Posts: 2 Rating: (2) |
Hello, we had the same problem on some of our Win 10 computers, after Microsoft Updates running For us the solution with repairing the MS Access Database Engine as described under It was not necessary to uninstall any Windows Updates. Hope this is helpful if you don't have KB4484127 installed on the computer with this issue. Best regards, |
This contribution was helpful to3 thankful Users |
11/22/2019 2:21 PM | |
Joined: 4/28/2015 Last visit: 10/6/2021 Posts: 1 Rating: (1) |
Hello AutoGen_8970897, i needed to uninstall and reinstal the MS Access Database Engine 2010 ("ACERedist.msi" file from the thx Best regards.
|
Last edited by: AutoGen_686506 at: 11/22/2019 14:34:29Last edited by: AutoGen_686506 at: 11/22/2019 14:38:44 |
|
This contribution was helpful to2 thankful Users |
Follow us on