4/9/2020 7:15 PM | |
Joined: 8/23/2019 Last visit: 3/27/2024 Posts: 58 Rating: (0) |
Hello Every one, I have project for Flying Punch & Cutting Application. My project built and compiled is normally, It's doesn't have error or warming. I download the project to PLC then I got error in LED on PLC. I try to diagnostic the project, So I got on the attachment below. I try to figure out them on these pictures. On this project, I used PLC S7 1200 1214 C and Sinamics V90 (Servo Drive). I m still looking for solution make tiral/error and read more siemens application technical on this forum. Am I did wrong use profinet on this project or profibus connected alternatively? So please anybody who can help me to make it working normally. SSI AttachmentError Topology View PLC & Sinamics Servo.pdf (80 Downloads) |
Follow us on