Industry Online Support
Technical Forum
7/31/2017 5:35 AM | |
Posts: 8 Rating: (0) |
hello guys, I am trying to add a new Simocode object via CiR function in my project HW page, complie is ok, but when I download the project, error 'Error in address parameters of the distributed I/O during CiR' occured. I followed this steps: 1. Copy existed Simocde object 631P742A(Profibus address 70), then select DP master line(2) and paste the object, and change the object name to match a new motor. 2. Change the profibus address to a new one, for example No.49 which is avaliable, then change the I/O address to avaliable one, for this case Input 2212..2215, output 2212..2213. 3. Complie and download Does anyone know what`s wrong with it? Thank you in advance. BR/Li AttachmentError pictures.zip (159 Downloads) |
7/31/2017 5:36 AM | |
Posts: 8 Rating: (0) |
Here is my CPU HW file. AttachmentHW_631ctl101.zip (165 Downloads) |
Follow us on