1/26/2021 1:31 PM | |
Posts: 31 Rating: (0) |
Hello, I want to install GSDML-V2.35-portGmbH-irj45-20200717.xml in TIA Portal V13 SP2 Update 4, but when I do that, I received next error: General GSD Error: Check-Number: 0x00010026_8,Message: The 'schemaLocation' attribute does not reference the appropriate schema file.,Line: 9,XPath: //ISO15745Profile/@xsi:schemaLocation[.='http://www.profibus.com/GSDML/2003/11/DeviceProfile ..\xsd\GSDML-DeviceProfile-v2.34.xsd'],
AttachmentGSDML-V2.35-portGmbH-irj45-20200717.zip (197 Downloads) |
Last edited by: redans.eu at: 01/26/2021 13:32:02 |
|
1/26/2021 3:32 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello redans.eu I think the version of the GSDML-Scheme is not compatible with your STEP 7 (TIA Portal) V13. See the table of the FAQ the currently supported versions of the GSD files with reference to the TIA Portal. "How do you install a GSD file and which GSD file version is released for which version of STEP 7 (TIA Portal)?" With best regards |
This contribution was helpful to2 thankful Users |
Follow us on