(0)
 (0)| 2/1/2019 1:18 PM | |
| Posts: 31 Rating: 
 | Need help. The situation: CPU 1214C DC \ DC \ Rly, analog and discrete modules. WinCC RT Professional (128 PowerTags) v14 sp1 update3, WindowsServer2016, TIA Portal v14 sp1 update3, WinCC Professional and STEP 7 Basic v14 sp3 update 3 There is a project: 1cpu, WinCCRT Professional 14, PC station In which you need to integrate the OPC server: - the OPC server is added to the PC station (the Device configuration already contains the IE general (192.168.1.2) and WinCC RT Professional 14) - an S7 connection is created from the OPC server to the PLC (there is already an HMI connection between WinCC and CPU) Compilation of PC station is successful only if the properties of the OPC server are: General tab - S7 - OPC symbols None option is selected (no tags selected). If you select All or Configured, then when compiling, the error TIA Portal "compilation of the hardware configuration failed (00ec)". At the same time, TIA Portal has crashing and closing. There is a record in the saved Diagnostic reports - Error while creating the 'TypeInfoSdb3127' (the screenshot is attached) UPD: This project was created on another computer and then copied to current PC. At that PC, where project was created, compilation of OPC server is OK. I think it is important information. Attachment0-02-05-b1482f841668962045cb5dc088210b5fac04f45a3658df711ab0c990145069e1_70bc141d.jpg (285 Downloads) | 
| Last edited by: 4phh at: 2/3/2019 1:29:52 PMLast edited by: 4phh at: 2/4/2019 12:27:36 PM | |
| 2/4/2019 2:42 PM | |
| Posts: 31 Rating: 
 | Screenshot of error after compilation. "SDB3100 for target OPC_Server_1 was generated successfully" Attachment0-02-05-7e0d186d2a64bbc7232dca9b16eef0c7481b068dcde4224a3540903fe0e95764_debd47d2.jpg (300 Downloads) | 
Follow us on