6/12/2018 9:10 AM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
Hello, I can not convert a project from v13 to v14 SP1. I attach the error log. Somebody can help me? Thank you. ------------------------------------------------------------------------------------------ AttachmentConversionLog_13.0.1.0_to_14.0.0.0[9].pdf (458 Downloads) |
Last edited by: The Helping Hand at: 6/12/2018 1:45:24 PMNew subject after splitting |
|
6/12/2018 2:27 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi radu83, first get the latest version of your SW: SIMATIC STEP 7 including PLCSIM V13 SP2 TRIAL download SIMATIC STEP 7 including PLCSIM V14 SP1 TRIAL download Updates for STEP 7 V14 SP1 and WinCC V14 SP1 If your SW is up to date, it should work without problems. regards, |
FCK WAR! |
|
6/13/2018 8:14 AM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
The next picture because I can't attach more than one file |
6/13/2018 8:14 AM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
the last picture |
6/13/2018 9:01 AM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
For a new empty project made in TIA v13 works but i can't upgrade my old project made in TIA v13 to TIA v14. I have in my old project: - PLC device -HMI device - G120C device If I delete the HMI device I can open the project but I need also the HMI device in my upgraded project. I try to put the HMI device into a global library and open this library with TIA v14. The result is the same error on upgrade. I attach the error log. Thank you. AttachmentConversionLog_13.0.1.0_to_14.0.0.0[9].pdf (408 Downloads) |
Last edited by: radu83 at: 6/13/2018 9:19:58 AM |
|
6/13/2018 9:33 AM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
The update stops at 75%. I save the error log and attach here. Thank you. AttachmentConversionLog_13.0.1.0_to_14.0.0.0[7].docx (422 Downloads) |
Follow us on