Industry Online Support
Technical Forum
12/22/2011 10:42 AM | |
Posts: 5 Rating: (0) |
Dear Experts We have purchased the S7-OpenModbus/TCP Redundant v2.0 function block library (Part No. 2XV9450-1MB11) to use with PCS7 v7.1 SP3 project, H system AS comms to Modcon packaged plant. I am having trouble using the block because of an issue with FC60, when I try to drag the blocks into my project I get an error message (attached) relating to FC60. I have checked I have the correctversion fo FC60 and it should be compatible according to the installion manualpage 1-2 & 3-11. Has anyone had and solved this problem or can anyone refer me to a solution?
Best Regards Paul B AttachmentMB_CPSRV Error.pdf (238 Downloads) |
12/22/2011 11:14 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
What kind of blocks do you have in CP_400 there? Best regards, Hristo MIhalev |
12/22/2011 10:08 PM | |
Posts: 433 Rating: (48) |
Hi, this is a problem of different versions of FC50 and FC60. You must update the blocks in the library. Tomcat |
Follow us on