10/14/2019 10:12 AM | |
Joined: 9/27/2018 Last visit: 5/14/2024 Posts: 10 Rating: (0) |
Hello at all, i'm trying to migrate a project from Step7 V5.6 Sp5 to TIA V13 SP1 upd9. I use this DB to eschange data from the PLC to the SIMOTION. But when i compile the consistency of the project it's all ok, 0 warning and 0 error. i've already tryied also to do a save as with the Save with re orginasation (slow) but nothing, all the time this message appear. Did someone have the solution for this Problem?. Thank you at all edit: my final "destination" is TIA V14 SP1 so now i've tryied to convert directly to it but it appear the same error. |
Last edited by: Sipti97 at: 10/14/2019 11:05:09 |
|
10/14/2019 10:17 AM | |
Joined: 7/9/2015 Last visit: 5/14/2024 Posts: 3831 Rating: (557)
|
Hi, please check the steps described in the following FAQ: What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?Regards, Towome |
|
|
10/14/2019 10:29 AM | |
Joined: 9/27/2018 Last visit: 5/14/2024 Posts: 10 Rating: (0) |
Hello, thank you for the answer. |
Last edited by: Sipti97 at: 10/14/2019 10:29:54 |
|
10/16/2019 4:00 PM | |
Joined: 7/7/2010 Last visit: 5/13/2024 Posts: 14710 Rating: (2363)
|
You should be able to export the DB to a text file (I would probably name it DB20_migrate.scl or something similar). Then in the TIA Portal project, use the external source portion of the project tree to bring DB20 back into the project after migration.
|
science guy |
|
Follow us on