1/2/2017 9:05 AM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
Hello Everyone there is a plc simulator which i am building Is there any problem with the CPU & I/O Modules arrangement I am using The CPU and the Base units are arranged in the manner listed below 1. SIMATIC ET 200SP CPU1512SP-1 PN / 2. DI 16X24 VDC mounted on A0 Base unit(Light Base unit)/ 3. DQ 16x24vdc/0.5 A Mounted on A0 Base Unit (Light Base unit)/ 4. AI 4X U/I 2-WIRE Mounted on A1 Base Unit(Light Base unit)/ 5. AQ 4XU/I Mounted on A1 Base Unit(Light Base unit ) All the base units being used are light colored Base Unit, Could this be the Problem? Please see the picture attached for all the other details . I am having an error on the CPU; ER LED on the CPU is blinking in red . Attachment1512SP-1PN.zip (334 Downloads) |
Last edited by: plc_317 at: 1/2/2017 10:15:45 AMWith kind regards... |
|
1/2/2017 10:05 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi plc_317, as Christoph already said, light base unit need to be configured as light base units. That means that every BU enables a new potential group.
Have a look to the manual: SIMATIC ET 200SP Manual Collection 1. manual: Basic Information - ET200SP Distributed IO System - Chapter 3 hope this helps, regards, |
FCK WAR! |
|
1/2/2017 10:07 AM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
Hi Christoph, I have changed the Base unit to light base unit the Digital Input module which is right to the CPU shows error Input output data not available CPU diagnostic Buffer says -User data Failure of Hardware components AttachmentAfter changing base unit to Light colour.zip (264 Downloads) |
Last edited by: plc_317 at: 1/2/2017 10:14:45 AMWith kind regards... |
|
1/2/2017 10:13 AM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
Hi mops04 , Yes all the base units are light coloured , from the manual i come to know that the light coloured base unit will be used for different potentials but in this simulator i am using only 24 volts for the Digital input and digital output and 10 volts for the Analog input and output . the power supply to all the four I/O Modules is 24 volts DC
|
Last edited by: plc_317 at: 1/2/2017 10:17:29 AMWith kind regards... |
|
1/2/2017 10:27 AM | |
Joined: 12/28/2016 Last visit: 12/22/2023 Posts: 364 Rating: (6) |
Hi Christoph , there is the server module at the end . please also see the attached diagnostic buffer file , the year is 2012 but it is current because the date time has not been set AttachmentDiagnostics.txt (279 Downloads) |
Last edited by: plc_317 at: 1/2/2017 10:27:51 AMWith kind regards... |
|
Follow us on