6/5/2021 12:32 PM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating: (0) |
Dear Expert, I want to configure S7-400H CPU with ET200Sp station. In ET200Sp stations i have to configure F-DI, F-DQ, And f-ai modules. But in the hardware catalogue i can only find F-DI & F-DQ modules. There is no F-AI modules in the hardware catalogue. So how can i configure F-AI (6ES7136-6AA00-0CA1) in simatic manager with s7-400H CPU. And i can configure the F-AI modules in Tia portal but it will not work for me as i have 400H CPU which can only be configured with simatic manager. My simatic manager version : V5.6+SP1+HF5 s7 distributed safety programming version : v5.4+sp5 s7 f configuration pack : v5.5+sp13 Please suggest me how to configure F-AI(6ES7136-6AA00-0CA1) modules in simatic manager. Attachment is the screenshot of my HW configuration and simatic manager software component. AttachmentHW&SW_COMPONENT.zip (223 Downloads) |
6/7/2021 9:39 AM | |
Joined: 3/11/2019 Last visit: 5/8/2024 Posts: 1408 Rating: (255) |
Dear RKB202, the F-AI should be included in the latest GSDML file. But in this case, the complete ET200SP station has to be configured via GSDML (GSD-folder). PROFINET GSD files: I/O - ET 200SPmaybe this helps regards sancruz |
Last edited by: sancruz at: 06/07/2021 09:40:46Last edited by: sancruz at: 06/07/2021 09:42:24Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on