6/1/2020 1:36 PM | |
Joined: 2/16/2015 Last visit: 5/6/2024 Posts: 13 Rating: (0) |
Hey, I would like to use ET200SP for distributed I/O with profinet in my project. However when i was using TIA selection tool i noticed different module types as in Basic, Standard, High Speed And High Feature for both Interface and the module. I researched and came across this link. However it was not helpful at all, as i was not able to understand the feature differences between them. I would be glad if anyone could illustrate differences between BA,ST,HS and HF Interfaces and modules with an example? Thanks! |
Follow us on